Declaration of accessibility
Danfoss endeavors to make its website accessible in accordance with the Accessibility Reinforcement Act (BFSG) and the Ordinance to the Accessibility Reinforcement Act (BFSGV). This declaration applies to https://discover-drives.danfoss.com/.
Description of the service
Our website provides information on modern drive technology and automation.
You can find out about technical solutions on our website, for example about devices that control motors and save energy.
You can view practical examples on our website. These show how the technology is used in different areas, for example in buildings or in industry.
You can read tips and knowledge about energy efficiency and technology on our website.
You can use an interactive online tool on our website. This allows you to discover potential energy savings in buildings.
You can register on our website for further information and request an information package or contact experts.
How our website meets accessibility requirements
Status of compatibility with the requirements
Our products and services can be found, accessed and used by people with disabilities in the usual way, without any particular difficulty and generally without assistance.
Our website is largely compatible with the BFSG and the BFSGV. However, there are still some barriers on our pages that we are actively working on and want to remove in the future. The following exceptions and incompatibilities exist:
The following contents are not barrier-free as they are not compatible with the underlying harmonized standard EN 301 549:
- There are images without captions on individual pages. It is difficult to navigate to the images with screen readers.
- There are links without link text on several pages.
- The contrast between text and background is too low on several pages.
- There are ‘iframe’ elements without labeling on individual pages. Navigation with screen readers to the iframes is difficult.
- There are form fields without labels on individual pages. It is difficult to navigate to the form fields with screen readers.
- There are invalid aria attribute values on individual pages. These are not recognized by screen readers and are therefore not displayed correctly.
- On individual pages, there are elements with the Aria-hidden attribute that can be focused at the same time. This means that these elements are accessible for assistive technologies, even though they should be hidden.
- There are lists on individual pages that contain elements that do not belong in lists. As a result, the lists may not be output correctly by assistive technologies.
This declaration was created on 06.05.2026. The declaration was created using the Eye-Able technology of Web Inclusion GmbH. Eye-Able Report – a product of Web Inclusion GmbH – has gone through all machine-verifiable test steps.
This declaration was last reviewed on 06.05.2026.
Contact details
You can report any difficulties in accessing the content of the website to us at:
info@danfoss.de
Market surveillance authority
The contact details of the market surveillance authority responsible for us are as follows:
MLBF AöR
Marktüberwachungsstelle der Länder für die Barrierefreiheit von Produkten und Dienstleistungen
Carl-Miller-Str. 6
39112 Magdeburg
MLBF@ms.sachsen-anhalt.de
Tel.: 0391 567 6970
Disclaimer
The automatic check of the web content was carried out on: 06.05.2026. The Google Chrome browser version 136.0.7103.92 was used for the web content when called up by Eye-Able. We guarantee the accuracy of the information provided for the tested application version under the specified browser and operating system parameters. If different versions or environments are used, a different presentation is possible, which may deviate from the results given here. For a complete check, manual tests by the website operator are also recommended.