Energy efficiency is an important factor when selecting electrical appliances. Energy efficiency class is a system that divides electrical appliances into different classes based on their energy efficiency. The higher the efficiency class, the more efficient the appliance is in terms of energy consumption and the lower the emission of propellant gases. There are various labels that indicate how much energy an appliance consumes. It is important that such labels are taken into account when purchasing electrical appliances.